AXIS#.UTWTHRESH

Description

This parameter returns the under temperature warning threshold of the power circuit for the specified axis. The value depends on the drive model. It is programmed in the drive and cannot be changed.

General Information

Type

Read Only

Units

degC

Range

N/A

Default Value

N/A

Data Type

Float

Industrial Ethernet Information

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5030

1

5030 (0x13a6)

AXIS1.UTWTHRESH

Signed32

Read Only

Yes

70566

2

5030 (0x13a6)

AXIS2.UTWTHRESH

Signed32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.UTWTHRESH

5030

Float

Read Only

-